STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 rise/fall shape

Hi, guys. I boughtSTM32F446RE, mbed-Enabled Development Nucleo STM32F4 MCU 32-Bit ARM® Cortex®-M4 Embedded Evaluation Board (NUCLEO-F446RE)https://www.digikey.com/product-detail/en/stmicroelectronics/NUCLEO-F446RE/497-15882-ND/53477128MHz ±10ppm Crys...

0690X000006DMAAQA4.png 0690X000006DMAFQA4.png 0690X000006DMAKQA4.jpg 0690X000006DMAPQA4.jpg
Matthew K by Associate II
  • 1276 Views
  • 1 replies
  • 0 kudos

what is the sampling time in ADC ?

I am using STM32F446 and I see 15 cycles for 12 bit ADC which gives 1.5 Msps for 180 Mhz clockBut I see on the bottom sampling time from 3 cycles to 480 cycles under something called rank.does it means that it would actualy do one sample in 3 cycles ...

MNapi by Senior III
  • 10465 Views
  • 4 replies
  • 0 kudos

Trigger ADC by timer

I'm having some difficulty getting this to work. This post is a very good description of the my confusion: https://community.st.com/s/question/0D50X00009XkghxSAB/triggering-adc-sampling-by-timer-eventsHowever the conclusion is not helpful. TRGO upda...

Lee3 by Associate III
  • 2308 Views
  • 4 replies
  • 0 kudos

ST-LINK V2 Can not connect to target! Help Me!!

Posted on August 22, 2016 at 14:52Hi All,Connect the pins were as follows: SWD ST-LINK V2 and between MCU.1:VDD - VDD3:GND - GND7:SWDIO - PA13_SWDIO 9:SWCLK - PA14_SWCLKPDR_ON: 10k pull-upBOOT0: 10k pull-downBYPASS_REG: 10k pull-downVCAP: 2.2uF GNDV...

sim20 by Associate II
  • 2768 Views
  • 6 replies
  • 0 kudos

Resolved! Beginner problems with 2xSPI and RTC

Hello, may someone help me with these peripherals? I have never used them on any ARM.I am using STM32F051C6T8 in this project.My setup, I have two shift register chains connected to SPI peripherals. I am using two peripherals, because two types of re...

Output Two ADC Channels Over UART

I'm using the nucelo STM32F446RE dev board and attempting to output two ADC channels over UART (technically I think it's USART). I Can see in the debug tab that I'm reading the ADC channels correctly. I had been reading out one channel over UART 2 (t...

PAbdu by Associate II
  • 1872 Views
  • 2 replies
  • 0 kudos

How to create an fsdata.c file

trying to create a simple web page. I am using an fsdata.c file from one of the example projects and everything seems to be working. Now, I created a simple html file and need to convert it to an fsdata.c file. I have looked up this topic at vario...

IAgui by Associate III
  • 5188 Views
  • 7 replies
  • 5 kudos

STM32F7, QUADSPI and the data cache - odd behaviour

Posted on June 12, 2018 at 12:41Hi all,I have a board using the STM32F765, which uses the QSPI interface to fetch data from an FPGA. The normal sequence of operation is: A timer in the FPGA causes it to perform a sequence of events which produce a ...

andy by Associate III
  • 14587 Views
  • 32 replies
  • 0 kudos