cancel
Showing results for 
Search instead for 
Did you mean: 

I have tried changing the GPIO output speed and then toggled the output and monitored it on a scope. There is a slight increase in rise time with the speed set to 50MHz, but otherwise very little difference. Why is this?

MCade
Associate
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

Which mcu?

Try to load the output with significant capacitance, tens of pF. Also, switch on the compensation cell, if your mcu has one.

JW

Bob S
Super User

What kind of load to you have on that pin? Is it connected to anything? Depending on the load you may not see any (or much) difference. For example, a pin with no connection or one driving a high-impedence/low capacitance load won't show much difference. A pin driving a low impedence and/or high capacitance load will show a big difference.