STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GUI Implementation for STM32

HI,I have a working code on STM32 NUCLEO-L452RE, which captures two Analog signals, and calculates their arctan. Currently I can visualize these signals in STMStudioI want to plot these signals as well as their ArcTan in a GUI/Dashboard that is clean...

AMoha.81 by Associate II
  • 1506 Views
  • 1 replies
  • 0 kudos

I am using STM32F051R6 series microcontroller for my project, i am unable to configure PC1 for port interrupt .

hi,I am using STM32F051R6 series micro controller for my project, i am unable to configure PC1 for port interrupt . I am sharing my configuration below#include "stm32f0xx.h"         // Device header#include "RTE_Components.h"       // Component selec...

Amal Babu by Associate III
  • 1802 Views
  • 3 replies
  • 0 kudos

CAN communication using STMF103

I am new with CAN bus implementation,can somebody point me in right direction?Example project would be the best.Thank youAlexei

ATikh by Associate II
  • 1886 Views
  • 4 replies
  • 0 kudos

Resolved! Stm32f4: Program Erased on Power Cycle -- SOLVED

First post on the forum...I’m currently programming a custom PCB with an Stm32f446ret6 for an uC. Using an SWD interface and System Workbench the program uploads fine. However when I disconnect the board, and then hook it up to an external P.S. the p...

dlepe by Associate II
  • 5578 Views
  • 6 replies
  • 0 kudos

Wrong Data send after correct Addr with I2C

Hi,I'm still having trouble with my I2C communication. I'm using the Bus as Master, at the moment without any Slave. After sending the Device Addr, which is transmitted correctly to the ouput (checked with logic analyser) I send data which is then pu...

0690X000006DTALQA4.png 0690X000006DTAGQA4.png
uli stone by Associate II
  • 3117 Views
  • 6 replies
  • 0 kudos