cancel
Showing results for 
Search instead for 
Did you mean: 

Can complementary timer pins be used as inputs?

AKuch.0
Associate

Hello,

I'm designing a PCB with an interface to an existing STM32769 board.

I would like to use one of the STM32 timer inputs to trigger a timer. When the timer reaches its "compare" value it should trigger a DMA request for an SPI transaction.

According to the reference manual, in order to send a DMA request for SPI, I have to use DMA2. The only timers that can send a request to DMA2 are TIM1 and TIM8.

Now, the only available pin that I have from this 2 timers is a complementary output TIM8_CH1N.

So my question is: can a pin whose alternate function is a complementary timer output also be used as a regular timer input?

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

No.

JW