STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Parallel flash operations on STM32H743

There are multiple references in the documentation that allude to being able to do two flash operations in parallel on the STM32H743 as long as you are doing these operations on different banks.For example, the reference manual RM0433 Section 3.2 sta...

ST User by Associate III
  • 1985 Views
  • 3 replies
  • 0 kudos

Stm32f103 ir transmitter

Hi,I want to realize ir transmitter with pwm signal but i do not understand the basic principle of pwm ir transmitter. What is the right way for creating ir transmit signal with pwm? Which peripherals must be used for this( pwm, timer interrupts...?)

er3481 by Senior
  • 746 Views
  • 0 replies
  • 0 kudos

reading multiple adc channels, no dma

Posted on January 26, 2015 at 11:58 Hello List, I,m struggling with reading, without DMA, from multiple channels. Every, say, 10 msec I call: var1 = Get_ADC_Value(11); var2 = Get_ADC_Value(12); Both variables ALWAYS get ...

Sietse by Associate III
  • 3922 Views
  • 7 replies
  • 0 kudos

Memory requirements for STM32H743XI EVAL board.

Hi All,I'm trying to implement the eval board for a project seems like they have used a lot of different types of memory from HW perspective. I wanted to know what memory is being used for what purpose for this specific board so that I can change it ...

BBV by Associate II
  • 3014 Views
  • 6 replies
  • 0 kudos

Resolved! What's minimal possible jitter when using STM32 DAC with DMA?

Hi,I need to generate a special waveform via DAC on a STM32F446. DAC samples must be generated at about 240kHz but with minimal jitter. A DMA channel with timer trigger will provide the data from internal RAM or flash. What best case - minimal - jit...

MFuch by Associate
  • 2352 Views
  • 6 replies
  • 0 kudos

STM32 programming service

Hello everyone.I'd like to ask about the possibility of purchasing pre-programmed STM32 parts with our application.For now, we expect a low volume production in the mid term, but it is expected to grow around 1 year after product launch.Is it possibl...

jose_1. by Associate
  • 2776 Views
  • 6 replies
  • 0 kudos

STM32L071 VREFINT_DIV

Hello, my work mate made a design where we have to measure a low voltage in a smaller range (0-.120mV) on an Input.His assumption and hardware realization to meet the requirements based on datasheet DS10690 Rev 6. Here on page 63 you can find the ta...

Artur1 by Associate II
  • 1855 Views
  • 2 replies
  • 0 kudos