User Activity

Hi;Can not interrupt CAN BUS application?I'm using the following codevoid HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan){ HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &RxMessage, RxData);}
Posted on June 21, 2018 at 15:20Hi friends;I using CubeMx 4.26.0 and Atollic TrueSTUDIO� for STM32 Version: 9.0.0When I create a project, it creates it with a virtual folder.How can we solve this problem?#virtual-folder #cubemx
Posted on June 16, 2018 at 22:25Hi friends,The while loop does not work in the following function. Why could it be?For STM32F407VG;void US_BEKLE(uint16_t us){ uint16_t baslangic = (uint16_t)__HAL_TIM_GET_COUNTER(&htim1);while(((uint16_t)__HAL_TIM_GE...
Posted on March 08, 2018 at 10:32 Hi, Do you have an example of CAN BUS Communication can be done with the current version HAL and CubeMx? Regards Ramazan #can-bus Note: this post was migrated and contained many threaded conversations, so...
Posted on February 24, 2018 at 12:24Hi,Why is CubeMX not generating the syscall.c file?RegardsRamazan#syscalls.c