STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Reference manual RM0360 got a mistake

Posted on October 29, 2015 at 11:54In the last version of RM0360,page 722, there is no description about the unique ID. But following the instruction of RM0091 I have read the 96bits ID out in some of my F030C8T6s .These numbers from several chips a...

Fail to detect STM32F103VC

Hi, this is first STM project and previously i do not have experience in st microelectronics controller but in other 32bit controller's.Our project based on following hardware and tools:STM32F103VCTST-Link V2 original toolsEclipse IDECube programming...

SB1 by Associate II
  • 787 Views
  • 0 replies
  • 0 kudos

A problem with STM STudio

When I want to import variables from the .elf file (generated by the TrueStudio, inside the Debug folder) into the STM Studio software, I get the below error. When I press OK and bypass it, it shows a list of variables, but none of them gets importe...

0690X0000060PqeQAE.jpg

Can't build STM32F746 + LWIP project

I created a project for using the STM32F746 DISCOVERY board with LwIP utility (see image 1 and 2 ). As soon as the project was created i tried to build it but ended up not beeing able to do so and getting the following error(see image 3):Hope someone...

MEsco by Associate II
  • 2768 Views
  • 2 replies
  • 0 kudos

Disable/enable interrupts globally on STM32F746

Hello,just a simple question. We share some data between ISR and application on STM32F746 processor (no RTOS used). How can we disable interrupts globally while application accesses the shared variables? Afterwards interrupts should be enabled again....

TechMarc by Associate II
  • 2407 Views
  • 5 replies
  • 0 kudos

ADC Modes

FolksIs there a good resource for understanding various ADC modes in F303 family? There is much confusion about the terminology (regular versus injected, continuous versus discontinuous, etc.) The material presented in manual/datasheet are diffuse, v...

Amir1 by Associate II
  • 1467 Views
  • 3 replies
  • 0 kudos