Posted on March 22, 2017 at 14:12STM32L0 LSI oscillator stops after a system reset, like software reset or watchdog reset, but LSI is not stopped by exit from standby. What is the difference between exit from standby and other system reset?
He Clive,After carefully reading the manual , now I understand. If Boot 0 pin is 0, the only way to enter and stay in boot-loader is to configure STM32L083 in bank mode and make the code in both banks invalid.thanks,
Hi Clive,Thank you. this is the code I have tried, but it did not work. I put the code in SystemInit, which is executed right in the Reset handler of the flash memory, but there is no USB device enumerated in the PC and the code reset repeatedly.voi...