STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sending 9 bit data using SPI STM32F7

Hi I'm using STM32F7 series microcontroller. Is it possible to send 9 bit data using SPI? the reason is i have to send 8 bit data along with command bit (ie 9th bit). I have seen some option in datasheet like we can chose the data length between 4...

PBU by Associate III
  • 2988 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F091, GPIO, USART

If switching GPIOA mode from 'General purpose output' (set to 1) to Alternate function USART Tx:Will level of pin break down for a short time or will it stay rock solid at "1" ?Rem. One has to change MODERy from 01 to 10. One may go via 01 -> 00 -> 1...

JuM by Senior
  • 2051 Views
  • 4 replies
  • 0 kudos

Generation file Linker (xxxx_FLASH.ld) is empty

Posted on March 04, 2015 at 11:20Hi The latest version of CubeMx in Ubuntu generates (export TrueSTUDIO) file Linker (xxxx_FLASH.ld) empty. I have tested this on STM32L0 and STM32F4. In Windows it all works. Has anyone encountered this problem? B...

drake by Associate II
  • 2461 Views
  • 4 replies
  • 0 kudos

Connecting a DRAM to an STM32

Hello, all!I need to explore an option to connect a DRAM to an MCU, and still ahve at least 40 PIOs and 16 AIOs left. and would like your input:Is there a comprehensive tutorial on how to connect and use a DRAM with an STM32?Any specific keywords I s...

ISeed by Senior
  • 4799 Views
  • 8 replies
  • 0 kudos

STM32H750VB Quad-SPI questions

Hello,Due to so attractive price + some specific features, the H7 Value Line looks to me very attractive to take into a new design, but 128kB Flash is not enough for me, I have to take an external flash, which is QSPI. I have a few basic questions a...

Yevpator by Associate III
  • 4352 Views
  • 10 replies
  • 0 kudos