cancel
Showing results for 
Search instead for 
Did you mean: 

Why do I get DMA1->LISR FIFO error when I use direct mode with double buffer mode

esukh
Associate III

DMA1_Stream0->FCR = 0

DMA configured to work in double buffer direct mode.

And I get FEIF0 error interrupt flag?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
AVarg.19
Associate II

Same problem for me also ( but I don't use a double buffer).

The FEIFx bit is being set when the DMA stream is enabled(EN = 1) in the DMA_SxCR.

Interestingly, it seems to happen only with Memory to Peripheral transfer.

waclawek.jan
Super User

This is the expected behaviour in the 'F2/'F4/'F7 DMA, see the note in 4.3 Software sequence to enable DMA in AN4031.

In Direct mode, simply ignore this flag, i.e. don't enable DMA_SxFCR.FEIE.

JW