STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI reliability problem when transferring large amount of data

I'm building SPI slave based on STM32F750V8T6 MCU and I'm having problem loosing sync between master and slave. When I run test that is sending sync bytes, slave receive data from master, sync again and slave is returning data after some time master ...

RMlad by Associate
  • 1894 Views
  • 3 replies
  • 0 kudos

Resolved! Unable to receive UART data randomly

Hi, I'm using STM32L0 series and working on UART to communicate with other module and I had chosen the polling method because i know the device max response time and exact data what i'm going to receive. I was running my application for testing and i...

Resolved! PG0 EXTI0 interrupt HW bug in STM32H743ZI MCU

I use on STM32H743ZI-Nucleo PG0 as GPIO interrupt with Falling Edge. It works, I get INT triggered, but:an INT is also triggered - sometimes (once every 1000 falling edges) - on a raising edge. After several tests I am sure, this PG0 EXTI0 is randoml...

Hi all, am using stm32l4S5IT microcontroller for reading internal temperature ,VBAT and vref but not able to read the exact values of each one ,

Vref is giving - 5200- 5700 mv but my source is (3300) maxVBAT - 3600 mvTemp- 170 degreesnot able to get why it giving that difference and my configurations are as per the example cube libraryNote: my Vref value is using as VREFANALOG_VOLTAGE for VB...

Resolved! Features depending on Power Supply-Flash memory access

Hello,​I​n the datasheet for the STM32F423 , I see at the table 18 "Features depending on Power Supply range". I want to understand what will be the performance of the MCU if I power it with 1.8 V. I don't clearly understand the table. At the column ...

Yevpator by Associate III
  • 2127 Views
  • 2 replies
  • 0 kudos

is anybody familiar with STM32F446RE and external clock ?

I tried to sort through the manual. When I choose external clock do i actually connect anything to the PH0 and PH1 pins and what kind of oscillator.I see that there is already what looks like 8 MHz crystal is this one I am connecting when using exter...

MNapi by Senior III
  • 2453 Views
  • 4 replies
  • 0 kudos

Problem with duty cycle measurement

Hello everybody,I wanted to measure the duty cycle (tone) of a PWM signal with input capture mode. Unfortunately, it works only almost up to 65% of the duty cycle(Ton). otherwise will the T_off measured instead of Ton. does anyone have an idea what c...

Samuel1 by Associate III
  • 1511 Views
  • 1 replies
  • 0 kudos