STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H747 Dual Core (M7 + M4)

https://www.st.com/content/ccc/resource/sales_and_marketing/presentation/technology_presentation/group0/ca/b8/42/c4/e3/9f/40/2e/CES_2019_Amazon_Alexa_Home_Control/files/CES_2019_Amazon_Alexa_Home_Control.pdf/jcr:content/translations/en.CES_2019_Amazo...

Resolved! STM32L496QG Flash Loader demonstrator problems

I have STM32L496QG soldered on my PCB. I can use only Boot Loader via Serial COM port. I tried to use ST's Flash Loader Demonstrator, it doesn't work. I need some Windows -based software. What can you recommend?

AStre by Associate III
  • 1518 Views
  • 2 replies
  • 0 kudos

STM32_DAC_OUTPUT

Hallo everybody,i would like to generate analog signal (0-5 V) via DAC but the problem is the maximam voltage is 3.3 V . ist it possible to change some configuration to generate an analog signal with maximam voltage from 5 V? thanks #DAC​ #[Analog an...

Samuel1 by Associate III
  • 3582 Views
  • 6 replies
  • 0 kudos

STM32F030R8Tx ADC Problem?

I do not know if and what I am doing wrong. I am using CubeMX and a Nucleo 64-Board. This is the while inside the main:while (1) { if(HAL_ADC_PollForConversion(&hadc, 1000) == HAL_OK){ adc_value[i] = HAL_ADC_GetValue(&hadc); media += ((f...

EFons by Associate II
  • 2053 Views
  • 4 replies
  • 0 kudos

Resolved! SPI back to back writes

Hello,setting up STM32L412 SPI for 16 bit Spi transfer and doing:    uint16_t *SPI_DR = (uint16_t*)&SPI1->DR;   *SPI_DR = 0;//   while (~SPI1->SR & SPI_SR_TXE) {NutSleep(0);}   *SPI_DR = 0;results in only 16 bit shifted out. With the check for TXE e...