STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Typical ST's MCU for power electronics control

Hello, I would like to ask if you can suggest me ST's MCU with peripheral specialized for power electronics controll. I would like to use MCU for PSFB DC/DC converters, three phase inverters, active PFCs and other common power electronics topologies....

TZure by Associate
  • 849 Views
  • 0 replies
  • 0 kudos

stm32cube, usb host, hid mouse/keyboard

Posted on October 09, 2016 at 14:54hello, I've been trying to set up some basic usb comunication with a usb mouse using my stm32f4 discvery. there are no usb examples for my board so I went in to look at other boards. I generated a project with cube...

arnie1 by Associate
  • 6055 Views
  • 9 replies
  • 1 kudos

Timer cookbook example on STM32F303RE platform?

Hello,Has anyone succeeded in getting the timer cookbook examples (specifically the TIM_ExtCLK_ETR)working on the STM32F303RE? I've been beating my head against the wall for a while now and still haven't seen the light. I'm using the IAR Embedded ...

Should LSERDY assert with LSEBYP?

Hello,should LSERDY assert with LSEBYP?I have a SIT1533 (32.768 khz Mems ocsillator) connected to PC14/OSC32IN on a L412. I first reset the backup domain, than I enable LSEBYP and with next command I enable LSEON. On a cold start, where the SIT1533 m...

STM32F030 Buz

Hi,I am working on the STM32F030C6 MCU to develop the alarm Buzzer tone generation.I need to buzz the buzzer with different melody tones and also need to control it Volume.Can anyone please share and suggest me how do we achieve the above functionali...

K_P_D by Associate II
  • 4657 Views
  • 9 replies
  • 0 kudos

FD CAN doesn't work properly

What is the best way to set up FD CAN in classic mode on stm32 nucleo h743zi board?Currently, I'm using FDCAN with 16 Mhz frequency on the bus and I want to get 500kbit/s.My settings are:hfdcan1.Init.NominalPrescaler=2;hfdcan1.Init.NominalSyncJumpWid...

MKami.0 by Associate
  • 1237 Views
  • 1 replies
  • 0 kudos