STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

String compression for UART on STM32F7

Hi, I'm working on a project in which i need to send strings through UARTMy throughput is limited because i'm working with Xbees, so i want to compress my ascii strings (that are long 1024 bytes and with simple structure because they are in csv forma...

MMand.9 by Associate
  • 2001 Views
  • 4 replies
  • 0 kudos

Can STM32 read external FIFO through the FSMC interface?

I want to use FSMC to read external FIFO implemented in an FPGA. Since there is no mode of FSMC that can match FIFO interface exactly, so I want to use the modified synchronous multiplexed PSRAM mode. The plan is like thisA[25:16]: Ignored, don't ...

0690X000008vxMnQAI.png
RLee.7 by Associate
  • 1440 Views
  • 1 replies
  • 0 kudos

FMPI2C on STM32F407

Is it possible to use Fast mode I2C on STM32F407 ? I looked everywhere for the I2CX pins GPIO but Can't find them at all.

Resolved! Micro controller

Hi All,Can anyone suggest a STM controller supporting following features.1) 1 I2C Port.2) 4 UART Ports.3) 20 Gpios4) 1 RGB LED PinThanks,Ashok

ab.7 by Associate II
  • 1455 Views
  • 2 replies
  • 0 kudos

Cheap Evaluation Board with SD-Card

Is there a cheap eval board e.g. Nucleo-64 with an SD-card reader. Also A cheap shield for Nucelo-64 with SD-card socket would be ok.Its for a simple logger application but I am hesitant to make a board for only a uC Sensor and SD-Card.

stephan2 by Associate II
  • 1593 Views
  • 2 replies
  • 0 kudos

How to use SPI + DMA in Full Duplex Mode

Hey guys,I'm currently struggling to setup my SPI to work in Full Duplex Mode together with an DMA.I'm using 2 STM32F4 to communicate via SPI + DMAThe Initialization for both MCUs was created using STM32Cube.This is the generated Init Code for the ma...

JHeni by Associate II
  • 6255 Views
  • 3 replies
  • 0 kudos

want to use 'stm32f407' to communicate with Lin.

Hello.I want to use 'stm32f407' to communicate with Lin.There are many difficulties because there are no example sources.Only errors occur when data is sent.If anyone has succeeded in lin, please help me.Give me a simple example of sending and receiv...

HG LEE by Associate II
  • 778 Views
  • 0 replies
  • 0 kudos