cancel
Showing results for 
Search instead for 
Did you mean: 

Timer sample code for buzzer on STM32L432G

Titus Stalin
Associate II

Can you please share me timer sample code for STM32L432G board.

I have Sensortile board and would like to interface buzzer, so I need to add timer code to get timer cb to toggle the required frequency to get the proper buzzer sound.

Also please suggest if anything is available for buzzer.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Timer examples which should be portable can be found in the code repository

STM32Cube_FW_L4_V1.13.0\Projects\NUCLEO-L432KC\Examples\TIM\TIM_PWMOutput

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
S.Ma
Principal

Note: If you use a piezo buzzer, you could use 2 TIMER PWM channels in opposite phase to double the piezo alternative voltage amplitude...