The above designated code seems not to support STM32 CUBE IDE. It is based on the SW4STM32 and MDK-ARM platforms. Can anyone please direct me to the proper source? Or, is there a way to convert any of these to cube IDE? Thank you
Using: stm32l476 on the ST eval board, I set the CAN INT as follows: if (HAL_CAN_ActivateNotification(&CanHandle, CAN_IER_TMEIE | CAN_IER_FMPIE0 | CAN_IER_ERRIE | CAN_IER_EPVIE | CAN_IER_BOFIE) != HAL_OK) { /* Notification Error */ ...
Thank you! Will follow the instructions. Let me ask you another question while we're here: can you recommend me your favorite IAP application example for STM32 (F4 single flash bank if I may be particular :)?