STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Queries on QSPI, used MCU stm32l4kc

The MCU qspi peripheral is connected to serial NOR flash. Along with these connection the same qspi individual data pins are connected to 3 individual Altera FPGA for booting purpose.qspi clock is common for all 3 FPGA.The following operation which a...

Internal temperature sensor

I'm trying to read the internal temp sensor of a STM32F030F4Px but datasheet isn't clear about how to calculate it.Vsense = ( 1686 / 4095 ) * 3.3 = 1.35VTemp = ((1.43 - 1.35) / 4.3 ) + 30 = 30.01CIn the code example it isn't any clear because I got:...

STM32L471 ADC offset 0.1V?

The CPU is powered using 1.8V both on VDD as well as VDDA (4.7uH coil as well as 1n/100n/1u capacitors in power path).When I measure the Vbat pin (100n cap supporting) in the range 2V-3.6V using the ADC I always measure about 0.1V less than the volta...

michael.m by Associate II
  • 1491 Views
  • 3 replies
  • 0 kudos

Resolved! I am new to STM32L4R5ZI. I have tried to dump the blinking LED code in STM32L4R5ZI using Keil MDK Arm 5 then I am getting following error... Contents mismatch at: 08001000H (Flash=00H Required=31H) !

I have generated the code (LED PB7 GPIO_OUT) by using STM32Cube Mx for MDK ARM5. While loading the code , I am getting following error.Contents mismatch at: 08001000H (Flash=00H Required=31H) !I have resolve this issue by erasing the flash using ST-L...

DVENK by Associate
  • 1159 Views
  • 1 replies
  • 0 kudos

Supply current in unprogrammed state

How can I calculate the supply current of the MCU (STM32L471) in unprogrammed state? We use it in an ultra-low power application and need to know the battery drain during production and storage.

Why stm32H743zi has longer access time to GPIO interface?

I have two nucleo-144 boards, stm32F767zi and stm32H743zi. Both cortex-M7, pin compatible, and pretty close in AHBx (GPIO) clock, 216 vs 200 MHz.Testing TFT LCD display library, that required fast 8-bits access to the LCD data bus, I discovered that ...

MasterT by Lead
  • 1825 Views
  • 2 replies
  • 0 kudos