2018-11-14 2:19 AM
i made project using Truestudio IDE with CUBEMX.
and I send the project folder to another computer that other colleague use
it that computer, there is error . so i cannot use that project files
is there anything i have to do whenever copy the project folder to another computer?
thankyou
2018-11-14 2:29 AM
Doesn't TrueStudio support project import/export via version control management clients ?