STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FIFO question ?

Dear Members,How can I save FIFO ?I have a psedo code :for (i = 0; i < NUM_SAMPLES_TO_READ; i++) {Read FIFO_DATA;Save IR[15:8];Read FIFO_DATA;Save IR[7:0];Read FIFO_DATA;Save R[15:8];Read FIFO_DATA;Save R[7:0];}STOP;my code :   for(i=0;i<=number_samp...

What is the Best oscillator Value of HSE oscillator for STM32L476 such that the power consumption is minimum? How does the peripherals react to it?

I am using STM32L476.In it I am using MSI as a clock source, I want to switch to HSE as Clock Source, I want to know the best oscillator to use (4-48Hz) so that the power consumption is minimum, also I want to know if there would be any change in the...

HShah.14 by Associate
  • 787 Views
  • 0 replies
  • 0 kudos

Using SDRAM and STM32

Hello,My questions are as follows:1. Can I use DDR-SDRAM with FMC or should i use SDRAM only?2. Can I use two SDRAMs and control them with "Chip Select" pin? I want to use this SDRAM. This SDRAM is similar to used on the STM32F779EVAL board, but 512M...

Slh by Senior
  • 1183 Views
  • 2 replies
  • 0 kudos

USART3 initialization in stm32f103r8

#include "stm32f10x.h"void usartSetup (void);int SendChar ();int main(){ while(1) { usartSetup(); SendChar(); }}void usartSetup (void) {RCC->APB1ENR = 0x00040000; RCC->APB2ENR = 0x0000000C;  GPIOB->CRH  = 0x00000900; USART3->BRR = 0x340; USART3->CR1 ...

GS by Associate
  • 1176 Views
  • 1 replies
  • 0 kudos

STM32H743 ADC documentation issues

I posted the list below as a reply in: https://community.st.com/s/question/0D50X0000A7WOCGSQ4/where-can-i-find-the-adc-input-impedance-of-stm32h743-in-differential-and-singleended-configurationsbut the thread seems buried and I think these items shou...

STM32L4 SPI interface to Flash Memory Winbond W25Q80DV

I am trying to interface with the Winbond W25Q80DV which is a SPI flash memory chip. I am using the STM32L476VG development board. To test the connection I am first trying to read the manufacturing ID from the chip. Using an oscilloscope I am able t...

JDarg by Associate II
  • 4096 Views
  • 4 replies
  • 0 kudos