STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MDMA read from DTCM - transfer error

I'm trying to move an array from DTCM to SRAM1.So I use MDMA in as memery to memory config. It isn't my first time I got it running, but never used it to transfer data from/to TCM region.I want to copy array at 0x20000018 starting address (DTCM regio...

AB.17 by Associate II
  • 792 Views
  • 0 replies
  • 0 kudos

STM32L063C8U6 pinout

I have bought STM32L063C8U6 (version in UFQFPN 48 package) but I can not find pinout in datasheet. DS10090 version 7 does not mention any UFQFPN package.Also SMTCubeMX says that "cannot load this MCU). Is this version secret?Thanks for answer, Jiří ...

JNeto by Associate
  • 1178 Views
  • 2 replies
  • 0 kudos

Support for STM32TS60?

Hello,Is it possible to get technical support for STM32TS60? I have some specific questions and would also welcome project files / BSP.BRNiclas

NArnd by Associate III
  • 1009 Views
  • 2 replies
  • 0 kudos

interfacing SDMMC with stm32f765Vitx

hello,we are using emmc memory device (capacity -8GB) with the part no: sfem008gb.we are using 8bit data transfer mode .when we generating code with help of cubeMX it will give drivers for 2GB memory interface ,what are changes we need to do for 8G...

srikanth by Associate III
  • 1558 Views
  • 2 replies
  • 0 kudos

STM32L5 privilege mode

Hi Sir,I am reading STM32L5 user manual. I noticed the privileged mode and unprivileged mode, as well as security attribution. I want to know if this privileged mode related to arm-cortex m cpu privileged mode?​For example, cpu in unprivileged mode c...

XChen.6 by Associate
  • 2836 Views
  • 1 replies
  • 0 kudos

Resolved! How to move ISRs to ITCM RAM

Hello,I try to run an ISR (void TIM3_IRQHandler(void)) in the ITCM RAM area. I'm new with scatter-files. Anybody has an example?(NUCLEO-H743ZI, Keil uVision)RegardsJakob

STM32L433CCT6: VBAT current anomaly

I'm still having problems with VBAT current consumption. I've loaded my firmware and the processor behaves correctly in all other respects. I removed all components from the processor to insure that there are no sneak paths for parasitic current dra...

Blue pill: What is my sampling frequency ?

Hello,My adc clock is 140.625 KHzMy sample time is 239.5 CyclesSo my Conversion time = 239.5 Cycles + 12.5 Cycles = 251.5 Cycles.1 Cycle = 1/Adc Clock 1/140.625 KHz = 7.1uSSo total conversion time = 251.5 * 7.1uS = 1.78msi.e my sampling frequency = ...

KVenk.8 by Associate
  • 1531 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.