2019-01-15 2:56 AM
Hello, i have probem with backup registers, which are powered from VBAT pin on Dicsovery board.
First problem was CubeMX init, where i can't choose LSE source, because the value of clock box, was not active. I tried differend things like change txt code for CubeMX project, and after code generation, the value changed again.
So I left CubeMX, and change code, first i comment 2 lines with LSI :
// in
void SystemClock_Config(void)
{
...
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; // | RCC_OSCILLATORTYPE_LSI;
// RCC_OscInitStruct.LSIState = RCC_LSI_ON;
...
}next i add my init :
void LSE_test(void){
if (HAL_RTCEx_BKUPRead(&hrtc,RTC_BKP_DR0) != BKP_VALUE)
{
LSE_init();
MX_RTC_Init();
}else{
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWR_EnableBkUpAccess();
HAL_RTC_WaitForSynchro(&hrtc);
assert_param(IS_RTC_CLEAR_FLAG(RTC_ISR_ALRAF));
/* Clear the Flags in the RTC_ISR register */
RTC->ISR = (uint32_t)((uint32_t)(~((RTC_ISR_ALRAF | RTC_ISR_INIT)& 0x0001FFFF) | (uint32_t)(RTC->ISR & RTC_ISR_INIT)));
}
}
void LSE_init(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInit;
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.LSEState= RCC_LSE_ON;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_RTC;
PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
// and cubemx function :
void MX_RTC_Init(void)
{
RTC_TimeTypeDef sTime;
RTC_DateTypeDef sDate;
// Enable Power clock
__HAL_RCC_PWR_CLK_ENABLE();
// Enable access to Backup domain
HAL_PWR_EnableBkUpAccess();
// // Reset Backup domain
// __HAL_RCC_BACKUPRESET_FORCE();
// __HAL_RCC_BACKUPRESET_RELEASE();
/**Initialize RTC Only
*/
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = 127;
hrtc.Init.SynchPrediv = 255;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/* USER CODE BEGIN RTC_Init 2 */
/* USER CODE END RTC_Init 2 */
/**Initialize RTC and set the Time and Date
*/
sTime.Hours = 0x10;
sTime.Minutes = 0x15;
sTime.Seconds = 0x0;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/* USER CODE BEGIN RTC_Init 3 */
/* USER CODE END RTC_Init 3 */
sDate.WeekDay = RTC_WEEKDAY_FRIDAY;
sDate.Month = RTC_MONTH_JANUARY;
sDate.Date = 0x4;
sDate.Year = 0x19;
if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/* USER CODE BEGIN RTC_Init 4 */
__HAL_RCC_RTC_ENABLE();
HAL_RTCEx_BKUPWrite(&hrtc,RTC_BKP_DR0,BKP_VALUE);
/* USER CODE END RTC_Init 4 */
}As you can see, I tried to place the code in different places, because I found various configurations in forum posts.
I modeled on the StandardPheriph library to reproduce the code.
In the reference manual there is no recipe for the use of backup registers. I find only that in std_lib for f0 :
##### Backup Domain Access #####
===============================================================================
[..] After reset, the backup domain (RTC registers and RTC backup data
registers) is protected against possible unwanted write accesses.
[..] To enable access to the Backup Domain and RTC registers, proceed as follows:
(#) Enable the Power Controller (PWR) APB1 interface clock using the
RCC_APB1PeriphClockCmd() function.
(#) Enable access to Backup domain using the PWR_BackupAccessCmd() function.
(#) Select the RTC clock source using the RCC_RTCCLKConfig() function.
(#) Enable RTC Clock using the RCC_RTCCLKCmd() function.If you have some idea, what should I change, I will be grateful. Thanks!!