I use STM32CUBEMX 5.5.0 create code for Nucleo-G474RE, when I set PIN PC2 to GPIO_EXTI2, after create code, the code didn't create correct code, only create two lines for EXTI15_10_IRQn, how EXTI15_10_IRQn can handle PC2?
I used ST32Cube_FW_H7 V1.5.0 Nucleo H743Zi example code for Nucleo H743Zi, the LED2 doesn't work, I thought I got bad module, then I order again, second Nucleo doesn't work too.
Same clock source doesn't means "FDCAN1 and FDCAN2 must always be in clock sync", A7 and M4 running different frequency and instruction different.You can't assume this.For my experience, debug time you can not assume anything before confirm, otherwi...
Hello Berendi,I set GPIO with PU, (I use falling interrupt) it is better.But there are two question I can't fig out:The NVIC->ISER[0] have to set to 0x100 for GPIOC2, do you know where I can find the STM32G474 NVIC registers map?Even I change code f...