STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is it possible to interrupt the middle of a += operation?

I think I have proven now through tests that the and is clearly "YES". But, I'll still put this is as some awareness raising anyway. It might not be immediately obvious that an interrupted task can override the value of an interrupting task. Also, I'...

DJC by Senior
  • 1191 Views
  • 2 replies
  • 0 kudos

4 devices on I2C ?

Dear Members,I have 4 devices on I2C 1, 2LCD s and 2 Sensors,I tried to init 16x2 I2C LCD, it seems that it blocked all the process,Is it because of 3.3V databus ? Does it need 5V databus?HAL_StatusTypeDef LCD_SendInternal(uint8_t lcd_addr, uint8_t d...

CAN TxMailbox pending

Hi ,I am using 2 F103rb NUCLEO. My code works fine in LoopBack modeBut when I use in normal mode, the TransmitMailbox status is pending I cannot receive on the other boardThe transceiver I use is TJA1050I do put resistor between CAN H and L , 120ohmM...

Xzhan.2 by Associate II
  • 645 Views
  • 0 replies
  • 1 kudos

STM32G070RB8TX- Board Malfunctioning

I am using STMG32G070RB8TX for Programming the device is detected in TS link Utility but when i compile the compiler throws an error below is the description of the error.Error in final launch sequence:Error in initializing ST-LINK device.Reason: (25...

SBHAR.16 by Associate
  • 777 Views
  • 0 replies
  • 0 kudos

I am having problems with B_L475e-IOT01A and the wifi

I have tried using the client demo program to try to connect to my android server. I can tan an android phone, setup as a tcp client and talk to the tcp server without issue. When i try the demo board it cannot obtain an ip address. I have used all t...

PHedl by Associate
  • 554 Views
  • 0 replies
  • 0 kudos

Complementary output PWM low can not sink current

​I used TIM1 to generate complementary output PWM signals. The EGR register is used to generate a COMG event to update the output signals. The output waveforms are good. But I found the output can't absorb sink current when it is low, a 2k pull up re...

ZDu by Associate
  • 679 Views
  • 0 replies
  • 0 kudos

Couldn't able to freeze IWDG in stop 2 mode

Hi,Greetings,I would like to freeze the IWDG in stop 2 mode.Code is available here:// Read bit and regitster                           LOG_Print("Flash->OPTR Value(Before):%#x\n",READ_BIT(FLASH->OPTR, FLASH_OPTR_IWDG_STOP));                       ...

SPare.9 by Associate II
  • 698 Views
  • 0 replies
  • 1 kudos

Looking for SDIO + eMMC example (STM32F401)

Hi,I'm looking for an example with SDIO + eMMC (and not SD). Is there something like that ?I know that there are threads about it, but I have not found a solution.Does someone get eMMC working? Read/Write? Could you please share your code or help to ...

JCorn.2 by Associate II
  • 1161 Views
  • 2 replies
  • 0 kudos