STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H745i-disco uboot support or device tree

Hi,I'm curently working on a STM32H745i-disco and need to implement a uboot on it. It doesn't seem to be natively supported. I would like to know if there is a port on going or at least if you have somewhere the linux/uboot device tree for this board...

STM32H562 Digital vs Analog temperature sensor

HiWe are currently working on a new board with a STM32H562. As part of the design, we want to measure the temperature of the MCU. In the Datasheet of the STM32H562 I see the “Analog temperature sensor” (as I know it from other STM32) connected to the...

MMeie.3 by Associate III
  • 2473 Views
  • 5 replies
  • 5 kudos

Resolved! First call of timer expires immediately

Hi,I am trying to check if a button is pressed for 3s continuously using a timer which is started through an interrupt. The code for the same is attached below. The issue I am facing is the interrupt is immediately called when I press the button afte...

Resolved! Unusual high and nonlinear ADC offset

Hello everyone,I've been struggling with the ADC of a STM32G474QE on a custom board for some while now. I initially saw a discrepancy between an onboard NTC thermocouple and its measured ADC value. The measured Value (calculated to mV) was off by an ...

EE_21 by Associate II
  • 5750 Views
  • 4 replies
  • 0 kudos

Resolved! CAN Communication Issue

Hi, I am using STM32F446RE Nucleo and a Peak CAN Usb to test the CAN functionality of the microcontroller. I have connected the Microcontroller to a CAN Transceiver (TJA1050) and added a 120ohm resistor between the CANH and CANL line. I have attached...

Resolved! 5V FT pins vs. injection current on STM32G0

I am confused about the limits of the FT pins on this MCU. I think I understand the maximum voltage on an FT pin except FT_c is Vdd + 4V as long as no pulls are enabled. So with 3.3V Vdd the max voltage on most FT pins will be 8.3V is that correct? I...

Carl_G by Senior III
  • 1501 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 Bootloader: FAA DO-178 Certification?

Is the internal bootloader on the STM32H723 DO-178 certified?   It just dawned on me that the whole line of CPUs might be disqualified for aircraft use because the bootloader code "flies" with the aircraft and all such code must be certified to the l...

Niramas by Associate III
  • 6035 Views
  • 17 replies
  • 0 kudos

Resolved! STM32G431 I2C with HAL gets stuck in the interrupt

I am trying to use a G431 as an I2C device (slave). Unfortunately it can be made to latch up rather easily, getting stuck with an endlessly triggering I2C interrupt. It appears to be a flaw in the HAL code where it doesn't clear the interrupt flags, ...

qua by Senior
  • 2470 Views
  • 5 replies
  • 0 kudos