cancel
Showing results for 
Search instead for 
Did you mean: 

Flash Control Register ECC Interrupt Enable Setting has No Effect

NickFF
Associate II

I am attempting to temporarily disable Flash ECC interrupts, for the purpose of validating data stored on internal flash, and discovered that the ECC Interrupt Enable settings seem to have no effect.

I am using an STM32H743, and have used the code below to intentionally trigger ECC interrupts. I experience the same interrupt (HardFault_IRQ), with the same FLASHn_SR values when a byte with an ECC mismatch is read, whether or not FLASH_CR_SNECCERRIE and/or FLASH_CR_DBECCERRIE are set. I have verified the bit settings via ST-Link/V2 ISOL debugger both before and after the interrupt occurs, and I'm using STM32CubeIDE.

 // CODE FOR INTENTIONALLY TRIGGERING ECC ERROR
char dummy[32];
char * pointer = (char*) FLASH_BANK2_BASE;
flash_eraseSector(FLASH_SECTOR_TOTAL);
memset(dummy,0xAF,sizeof(dummy));
HAL_FLASH_Program(FLASH_TYPEPROGRAM_FLASHWORD, FLASH_BANK2_BASE, (uint32_t)dummy);
dummy[0] = *pointer; // does not trigger ECC interrupt
memset(dummy,0x5A,sizeof(dummy));
HAL_FLASH_Program(FLASH_TYPEPROGRAM_FLASHWORD, FLASH_BANK2_BASE, (uint32_t)dummy);
dummy[0] = *pointer; // triggers ECC interrupt

Does anyone know anything about this? Is there another register than must be used?

1 REPLY 1
Sarra.S
ST Employee

Hello @NickFF,

For the FLASH_CR_SNECCERRIE and FLASH_CR_DBECCERRIE interrupts to be effective, the LOCK2 bit should be cleared to 0.

Check: 

 

LOCK.PNG

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.