User Activity

Hi all, per AN3156 it states G0 series have USB DFU mode built-in the factory bootloader, so does it mean I won't have to configure the USB Device DFU Class in the CubeMX in order to make it work? Could I configure it into other classes (like CDC Vir...
Greetings,I tried to setup a L0 using SPI to connect with LSM6DSR, all codes are generated using CubeMX (also the driver code for LSM6DSR with X-CUBE-MEMS1)The weird thing is, when ever it tries to utilize SPI functions (Transmit, Receive, and Transm...
I am using the same schematics as the datasheet's typical application schematics sugguests. The EN and PWM pin were tied together with Vin. When I connect it to 12V power, It went steady for a couple of seconds then it starts to flash, it turns off a...
in STM8L151G3 the PA0, PB0 and PB4 is configured with pull-up under reset. I wonder if we can change it back to floating under reset?
I downloaded the blink LED demo from ST and loaded in that nucleo board to check out how things worked, soon I found out that every time when I pressed the "USER" Button (Connected to PE4), It won't be able to successfully switch to next blink patter...
Kudos from