STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

how can i get a character on telnet API

Hi,I've been coding for telnet console using ​API KEIL offer.I'm working on Telnet_Server_UIF.CPP which was created by example installer of KEIL.i can get strings via netTELNETs_ProcessCommand call back. this only gives me strings after hitting enter...

JLim.13 by Associate
  • 1283 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F207 was HangUp, at the GPIO Initial.

Hi.yesterday, my stm32 board run was good.today, I add to code​(printf...). but my board is hangup.I was check memory over. but, i use 25%.project.map    177 901 bytes of readonly code memory    54 396 bytes of readonly data memory    87 330 bytes of...

SYun by Associate
  • 1561 Views
  • 2 replies
  • 0 kudos

Resolved! How do I go from an integer value to a q31_t? Do I need to normalize the in32_t to a value between -1 and 1 and then pass to arm_pid_q31 to complete the calculation?

I am using the arm pid library and I do not know how to use the arm_pid_q31 call. I need to give it an error as a q31_t, however, I am not entirely sure how to go from an int32_t to a q31_t. Do I need to normalize the in32_t to a value between -1 and...

AIsma by Associate II
  • 5941 Views
  • 6 replies
  • 1 kudos

How to use same pin as gpio input and syswkup pin ?

I am using STM32L0Configured PA.0 as syswkup pin in cubemxBut i want to use it as gpio input for a push button while running the microcontroller and send it to standby mode.And while in sleep ,want to use same button to wakeit upIs it possible ?How t...

SA.17 by Associate III
  • 668 Views
  • 0 replies
  • 0 kudos

Invoking added performance using dual core

I have been driving CCD/CMOS linear arrays using PIC24s and have exceeded this processors 64mHz capability so i am seeking something much faster. I see that the STM32H7 MCU has a 480mHz clock and thought I would give it a try. It is a little uncl...

Resolved! X-NUCLEO-IDW01M1 examples don't work on NUCLEO-L476RG boards

Posted on March 25, 2017 at 16:28Hello STM Community. I am using the openstm32 System Workbench IDE and would like to play some of the https://my.st.com/content/my_st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/s...

business by Associate II
  • 2922 Views
  • 6 replies
  • 0 kudos

STM32H753 clock setting

Hi friends.I work with this chip STM32H753, but I set wrong clock. void SystemClock_Config(void) { uint32_t i;   // Enable HSE LL_RCC_HSE_Enable(); // Wait till HSE is ready while ((LL_RCC_HSE_IsReady()) == 0) ; //PLL1 - external quartz LL_R...

0690X0000098HHbQAM.png

Sampling rate L011 too slow

Hi there.I am trying to measure progress of signal with STM32L011F4. I start measuring on three ADC channels (two inputs and reference), 30 samples on each of them by one DMA request. Frequency for ADC is set to 16Mhz (Max), ADC clock prescaler set ...

JSkod by Associate
  • 1377 Views
  • 2 replies
  • 0 kudos

Not able to do Chip erase on STM32H750VBT6 Internal flash

Hi,I am new to STM32 H7. I designed 1 board using STM32H750VBT6. But when i try to erase internal flash using keil IDE, it is showing 'Flash Timeout: Reset the target and try it again'. I have attached the scrennshot of the error.

VAgga by Associate II
  • 7996 Views
  • 10 replies
  • 0 kudos