IrDA compliant library
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2012-05-08 3:56 PM
Posted on May 09, 2012 at 00:56
One of the areas I'm looking at with the STM32 is being able to transfer files (or at least data) from an IrDA dongle from Windows to the STM32. However, as I understand it, the STM32 only implements the PHY layer using SIR, and it's missing the other two mandatory layers (IrLAP and IrMP), which I'm assuming is software based.
Is there any library out there that I could use for the STM32 that is IrDA compliant and/or can interface with Windows? EDIT: Actually never mind. It took me a while to find out some folks make a raw IR to serial adapter, which would be even better in this case. #irda
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-02-20 10:26 PM
could you please share what "raw IR to serial adapter" to use?
i need a short range (10cm) wireless communication