STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H753 Revision V Migration

Hello,We currently have a board with the STM32H753XI Rev.Y MCU.We're building a new revision of the board, and saw that there is a new STM32H753 revision (Rev.V). This revision has significant changes.There is no new part number for the Rev.V devices...

Yan Rosh by Associate II
  • 1610 Views
  • 2 replies
  • 0 kudos

Problems with UART4 on the Nucleo-F429ZI

I'm working with the Nucleo-144 (STM32F429ZI) on a multi sensor system. I am developing using STM32CubeIDE.One of our sensors communicates over UART and we have broken out UART4 such that PC10 is TX and PC11 is RX. This configuration is suggested as...

jermat by Associate
  • 814 Views
  • 0 replies
  • 0 kudos

STM32L151 did not wake up from stop mode RTC

Hi Comunity. This is my code project code to enter to stop modeNVIC_InitTypeDef NVIC_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; /* Enable PWR APB1 Clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);   /* Allow access to R...

Hoang Loc by Associate II
  • 1227 Views
  • 1 replies
  • 0 kudos

Resolved! STM Flash Loader Demo does not recognize my NUCLEO-F767ZI

I am trying to use the built in boot-loader on my STM32F767. I wrote a simple app on my PC and I can get sensible answers from GET, GET VERSION, GET ID commands. But when I try to do a GO or a READ, the address (I have tries 0x00200000, 0x08000000 an...

KDuff.15 by Associate II
  • 1836 Views
  • 2 replies
  • 0 kudos

Resolved! stm32 uart Tx dma transmission doesn't work

I'm using the stm32f103 and I'm trying to send a text stored in SRAM via DMA to the USART 2 peripheral. My assumption is I'll turn on the usart2 TX dma ( DMAT )request whenever I need it and turn it off after the current transmission completes, (i.e...

ASeyo by Associate II
  • 4931 Views
  • 6 replies
  • 1 kudos

Reading ADC3 VREF, VBAT and VTEMPERATURE on NUCLEO-H743ZI with STM32H743xI MCU - Cannot find any H7 references to the VREFINT_CAL_ADDR to determine Factory burnt VREFINT_CAL value for VDD calculation; same with TEMPSENSOR_CAL1_ADDR and _CAL2_ADDR

I have managed to get ADC working in Interrupt mode and can read the three sensors values into a buffer called ADC3_VALUES[] on each of 3 callback events triggered by the ADC..../* USER CODE BEGIN 1 */void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* ...

SWood.8 by Associate III
  • 2015 Views
  • 2 replies
  • 0 kudos

Does input frequency matter for smooth digital calibration

Hi, does input frequency have effect on the smooth digital calibration period since in the documentation(screenshot attached) it says the calibration is performed during a cycle of 2 to the power of 20 which amounts to frequency of 32.768 x 32 . Does...

Ismet by Associate
  • 737 Views
  • 0 replies
  • 0 kudos