STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problem with timer and input capture, timer does not run

Does anyone have experience with getting the timer to run with input capture, I am unable to make the input capture function.I have a working system with STM32F03 (M0) devices initialization generated by CubeMX. Now I am testing an identical system w...

TMalt by Associate II
  • 3386 Views
  • 4 replies
  • 0 kudos

HardFault on STM32F765

Hi,My code is generating a HardFault condition, is not every single time it pass the main loop, but after the first 5s it stops.The Hardfault not happen every time in the same line, that is what have been so difficult to track down, but it always sto...

0690X000009YoaXQAS.png 0690X000009YoamQAC.png

ADC channel 0 with DMA ?

Dear Members,I tried to initialize ADC1 channel 0 with DMA but I got not output yet,Init code :ADC_HandleTypeDef hadc; DMA_HandleTypeDef hdma_adc;   /* ADC init function */ void MX_ADC_Init(void) { ADC_ChannelConfTypeDef sConfig = {0};   /**Confi...

Disabling Hex File Generation?

Setting up an embedded project with the Blinky Hello World project, and my build keeps making a .hex file when I don't really want it to. There isn't anything in the pre or post build steps that should be generating a .hex file (the way I found onli...

How to update the controller software in the field.

I am thinking about a new control unit for my project and want to use 2 STM32 controllersController 1: STM32F413 or maybe some lowpower STM32 with 6 Uart/USart•   Messurementso   10x ADCo   12x IO Outputso   4x pulse inputo   5 x different 485 and 23...

FloX by Associate II
  • 1154 Views
  • 1 replies
  • 0 kudos

Measure PWM Input Frequency from 0.016 Hz to 250 Hz

Greetings Everybody,I want to ready PWM Input Frequency from 0.016 Hz to 250 Hz. I tried a bit with PWM Input Capture and i can read up to 11 Hz . Is it possible to ready frequencies lower than this ?May be i might be doing some thing wrong in settin...

Resolved! Temperature sensor characteristics of STM32F407

As per table 69 under section 5.3.22 of datasheet STM32F405XX/407XX (DocID022152 Rev 8), the parameters of “Average slope�? (Avg_Slope) and “Voltage at 25°C�? are specified to be 2.5mV/°C and 0.76V, respectively. Does it imply the sensitivity to be 4...

TKumi by Associate
  • 3290 Views
  • 2 replies
  • 1 kudos