cancel
Showing results for 
Search instead for 
Did you mean: 

I am having trouble with the function HAL_QSPI_TRANSMIT().

MSimm.15
Associate

I am using the QSPI on my nucleo STM32F767zi  board to access a WINBOND FLASH chip.  I am using cubeMX 2.61 with IAR compiler 7.80. ​

I can access the FLASH chip using HAL_QSPI_COmmand(). I appear to get dat when I issue a command to read the chip and then use HAL_QSPI_Receive().

However, oscilloscope show that when I issue the  write command and then a HAL_QSPI_Transmit() function the command and address go out a second time. No data is sent on the bus for the actual writing even though the stm32f7xx_hal_qspi says the register is being loaded with my tx bytes.

The structure QSPI_CommandTypeDef is not explained in detail.  The examples in mxcube sample projects only cover internal memory operation. Any other sample code out there? HELP!!!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0