STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F429, external interrupt errata?

External interrupt errata?I have setup EXTI_Line12 and EXTI_Line14 to generate en interrupt.But the EXTI15_10_IRQHandler() fails to execute a second interrupt if it happens too close to the first interrupt.But it seems only happen when I use bit-band...

MSipo by Senior II
  • 1654 Views
  • 3 replies
  • 0 kudos

Resolved! Simple ADC example

I'm having trouble getting the ADC on a STM32L476VGT6 discovery board to work. If I run by configuration code then click the ADSTART bit in the debugger, everything works fine. If I set the ADSTART bit in code in real time, the conversion never fin...

AWolf.8 by Associate III
  • 2798 Views
  • 5 replies
  • 0 kudos

STM32F446 silicon revision 3?

In the STM32F446xC/E datasheet, DocID027107 Rev 6, footnote under Table 11. Alternate function says:1. The DCMI_VSYNC alternate function on PG9 is only available on silicon revision 3.However, neither DBGMCU_IDCODE description in RM0390 Rev 4, nor ST...