User Activity

Hello,We have developed a custom board having STM32F746NGHx MCU based of the design of the STM32F746G-DISCO board.We are using ST-Link Utility and ST LinkV3-SET Debugger in JTAG mode to flash.The board gets flashed and the program is executed after f...
Hello,We have developed a custom STM32 board using STM32F746G controller, with the hardware design based on STM32F746G-DISCO EVAL board.We are using TouchGFX for developing graphics.The debug interface we are using is JTAG, and the debugger we are us...
Hello,We want to use 32F723EDISCOVERY having Frida FRD154BP2902-CTP LCD display.On the TouchGFX designer it's application template is not available and also it's not listed in supported ST kits on the website. https://www.touchgfx.com/product/support...
Hello,We want to make a custom board having STM32 and supported by TouchGFX.We currently have been evaluating STM32L4R9I EVAL board and the controller used is STM32L4R9AI which is BGA package.For our custom board we want to use controller with LQFP p...
Hello,I want to display the current time in TouchGFX project.I am using TGFX 4.9.3 (using Keil IDE) and I want to use the Internal RTC to update set time.The issue is that the clock settings are already defined when the project is created.So I tried ...
Kudos from