STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Filtering ADC output with FIR ?

Dear Members,Dear Members,I got a FIR filter coefficient from matlab :/* General type conversion for MATLAB generated C-code */ #include "tmwtypes.h" /* * Expected path to tmwtypes.h * C:\Program Files\MATLAB\R2018b\extern\include\tmwtypes.h *...

BlueNRG-2 IIC error with reading more than 16 bytes

Hi, I am working on BlueNRG-2 and I need drive NFC-EERPOM(M24SR64). I tried to read from M24SR64, I got error when the reading bytes were more than 16.(It was ok <= 16 bytes), it stuck on the while loop as below. I put my readfunction and init func...

SZhan.5 by Associate
  • 1523 Views
  • 2 replies
  • 0 kudos

Get STM32F4 Software

Can you please help me to get quick link to download STM32479I-EVAL demonstration software? I can see related resources but unable to find the demonstration software.

TJagd by Associate
  • 965 Views
  • 1 replies
  • 0 kudos

STM32F4. Interrupt from DMA burst writing only once appears

MCU is STM32F405. I write data array to output pins using DMA mem to peripheral (DM2 stream6 channel0). Trigger is TIM1 CC1 event. Also I use DMA2 stream5 channel6 for write to TIM1 registers. Trigger is TIM1 UEV event. So the writing and interrupt D...

Alex Mach by Associate III
  • 3720 Views
  • 8 replies
  • 0 kudos

DAC in DMA not working?

dear all,I keep studing the STM32H7 architecture and this time I am trying to control a DAC using DMA which seems an easy task. However, in my case, the output is always at zero. I have used it without DMA and it works, therefore my HW debugging work...

Mdi c by Associate III
  • 1449 Views
  • 2 replies
  • 0 kudos

new vs malloc - surprising results with IAR

Hello,Recently I started using c++ application with STM32, and I encounter a very strange behavior:It seems that after 1-3 calls to new() operator the new operator call get hang somewhere into assembly. When I try to step into the problematic new cal...

ranran by Senior II
  • 961 Views
  • 1 replies
  • 0 kudos