STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

mpu6050 returns zero, I2C stm32f103

I am working with MPU6050 and STM32f103VE as master. When I wake up the sensor and ask for information it returns 3 bytes of zeroes and the protocol stops working. I only send the communication Part of my code to be more specific:void I2C_interface(v...

Delay in microseconds for stm32l0 cortex m0+

I Wanted to generate the microsecond delay function, I have tried below functions but these are not working, It will be good if someone knows the delay function.static inline void delay_us( uint32_t micros){   micros *= (SystemCoreClock / 1000000) / ...

Resolved! Cannot connect to STM32H753I_EVAL2 board anymore

I know it sounds like a dumb question but I cannot connect anymore to my STM32H753I_EVAL2 (that I've been using extensively for months). I checked the driver in Windows Peripheral Manager. It is properly installed and it shows the same driver DLL as ...

Gpeti by Senior II
  • 886 Views
  • 1 replies
  • 0 kudos

STM32l073CB internal RTC alarm

Hi,How to set alarm and read the alarm flag?I already write the RTC_ALRMAR = 0x85 to set alarm 5sec and mask sec. But the reading of ALRAF in RTC_ISR was not changed to 1 after it matched 5sec. Can U help me? I already set the RTC value with my homet...

Dprom by Associate II
  • 729 Views
  • 0 replies
  • 0 kudos

stm32f105 usart interrupt generated only once times.

when program started interrupt is called but its read only one character and repeatedly read same character.most time getting garbage value. RXNE Flag also set. my application is to handle data send by ATMEGA16 in while condition.program: voi...

vivek by Associate II
  • 1565 Views
  • 2 replies
  • 0 kudos

Are the STM32F301x4 and STM32F302x4 devices discontinued?

Hi everyone,This is a fairly straight forward question. The STM32F301x4 and STM32F302x4 are listed on DigiKey as a non-stock item but are still present on the website when searched. I was unable to find any reference manual for these parts as well. A...

SMcGr by Associate II
  • 1705 Views
  • 2 replies
  • 0 kudos