cancel
Showing results for 
Search instead for 
Did you mean: 

how can use same pin as MISO and GPIO interrupt simultaneously in STM32L073

VGoya
Associate II

I want to use same pin for SPI MISO and GPIO Interrupt.When I need to take data from SPI BUS then I want touse it as SPI MISO else want to use as GPIO Interrupt. How can I use same pin for both functions?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
S.Ma
Principal

You need to hack as CubeMX and HAL won't intuitively offer EXTI interrupt on an Alternate function pin.

The Reference manual shows that EXTI is an independent block.

Got this working on SPI SCK on STM32L4R

void SPIP_EnableSCK_EXTI(SPIP_t* pSPIP) {
  SYSCFG->EXTICR[0] &= ~(0xF<<4);
  SYSCFG->EXTICR[0] |= (3<<4);
  EXTI->IMR1 |= GPIO_PIN_1; // interrupt enable
  EXTI->RTSR1 |= GPIO_PIN_1; // rising sense
  EXTI->FTSR1 |= GPIO_PIN_1; // falling sense
// Above is to have EXTI on AF pin.
  __HAL_GPIO_EXTI_CLEAR_IT(pSPIP->pSCK->Init.Pin);
  __HAL_GPIO_EXTI_CLEAR_FLAG(pSPIP->pSCK->Init.Pin);
  //EXTI->IMR1 |= (1<<1);
  HAL_NVIC_SetPriority(EXTI1_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(EXTI1_IRQn);
}