STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 SPI with DMA using memory to start transfer

Dear all,I'm starting to use STM32H7 for a real-time project and my first task is to optimize the SPI communication. The final implementation will be a library that elaborates data from SPI and send the elaborated data in another SPI (like a pass-thr...

ARess by Associate
  • 2759 Views
  • 3 replies
  • 0 kudos

Can you use a unified firmware for dual core STM32H7x5?

I'd like to develop an application on the dual-core STM32H7 line.  To simplify development, I'd like to use the same firmware for both cores.  Is this possible?As I understand it, accessing the SCB->CPUID can tell me which core is running. Okay, so ...

TDK by Super User
  • 835 Views
  • 0 replies
  • 0 kudos

how to initialize stm32l496 RTC ?

I have just started working with Micro controller, I use stm32l496 .I want to init RTC with LSI clock source and HCLK is 2MHz from MSI source. I configure RTC in stm32 cubemx but RTC is not working i.e. the time is set correctly but does not increase...

alianvari by Associate III
  • 1416 Views
  • 0 replies
  • 0 kudos

Output Compare Mode for STM32F407 Discovery board

Hi,I am working on STM32F4 discovery board and I am trying to use output compare mode.and I have written the following code using peripheral registers.The application is Toggle the LED for every 1sec when output compare is matched.Here is the code. B...

Kumar B by Associate II
  • 2019 Views
  • 4 replies
  • 0 kudos

Resolved! Value of the hysteresis of the comparators nowhere to be found

Hello,Looking at the datasheet and the reference manual, I can't find the values of the hysteresis that can be used for the comparators, the datasheet simply states Low, Medium and High values, which is not very precise. Anyone knows the exact values...

LLouf by Associate II
  • 1296 Views
  • 1 replies
  • 0 kudos

Nucleo-H743zi ADC dual simultaneous with DMA example?

Hi,I am working with the Nucleo-H743zi. I am unable to get the DMA working in dual simultaneous mode. I see the ADC12_Common CDR registers are showing the ADC values properly, but my DMA never seems to fire.I can not find an example of ADC dual simul...

ATo by Associate II
  • 1329 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.