STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L0 Comparator interrupt.

Hello!I am trying to generate COMP2 interrupt on the rising edge on Input[+] of COMP2.Input[-] is conected to ground and Input[+] is connected to pull down resistor.What is strange that interrupt is generated only when Input[+] is connected to ground...

LMehm by Associate III
  • 641 Views
  • 0 replies
  • 0 kudos

STM32F446RE Mongoose

How to setup mongoose with STM32F446RE ?In mongoose browser window STM32F446RE not available.How to start program using mongoose for STM32F446REbelow i'm added mongoose board available on browser window

chum by Associate II
  • 1679 Views
  • 1 replies
  • 0 kudos

simple spi on F103 have little problem

hi i use two spi and connect together spi 1 send(Full D Master) and 2 receive(Full D slave ) all in dmaif i change send buffer, in receive first array not change. it was first init that send dma uint8_t TXBuf[]={0,1,2,3,4,5,6,7,8,9}; uint8_t RXBuf[10...

MacLaren by Associate III
  • 1244 Views
  • 1 replies
  • 0 kudos

What is the response for STM32H7 DFSDM in FastSinc mode?

The STM32H7 reference manual revision 6 gives the FastSinc response as:However this seems to make no sense. The first part is a normal sinc^2 filter, but the second part describes an impulse + delayed impulse, which results in a quite strange frequen...

0690X00000As7JwQAJ.png
jpa by Associate II
  • 1312 Views
  • 1 replies
  • 0 kudos

Hard fault issue while transmitting data on UART

Hi All,I config UART on interrupt, after receving data on UART simple sending data at that time hard fault occur.UART enabling code MX_GPIO_Init(); MX_DMA_Init(); MX_USART2_UART_Init(); MX_RTC_Init(); MX_SPI3_Init(); MX_TIM2_Init(); MX_TI...

0690X00000AsYS7QAN.jpg
ASaxe by Associate II
  • 2948 Views
  • 4 replies
  • 0 kudos

STM32L496 - Power OFF SRAM1 during Run Mode

I want to know if is possible power OFF the SRAM1 (256kb) and keep only SRAM2 (64kb) ON, during Run Mode. I know that is possible power OFF SRAM2 in Standby-Mode with the register PWR_CR3 (bit RRS). - Reference Manual pag. 187