STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H723VGT6 not connecting st-link v3

We are currently developing a new product using STM32H723VGT6 (LQFP100 package).We purchased 10 pieces, and during initial board bring-up, we are observing that several chips from the same lot are unable to communicate via SWD (Device ID read failure...

namyoung by Associate
  • 1300 Views
  • 2 replies
  • 0 kudos

STM32H5 high cycle flash read.

What is the correct way to read high cycle flash data.When i read address 0x916800 i get a Hard fault. Clearing and writing the this address works fine.With reading i have a problem. bank 2 has EDATA enabled for the last 2 pages. Can you give me a co...

MVanb.1 by Associate II
  • 2202 Views
  • 4 replies
  • 0 kudos

Pinout for the NUCLEO-F767ZI to use the HX711

Hello,I’m currently working on integrating the HX711 load cell amplifier with my NUCLEO-F767ZI development board. However, I’m having some difficulty determining which GPIO pins to use for the SCK (clock) and DT (data) lines.As I’m relatively new to ...

Apal by Associate
  • 1428 Views
  • 2 replies
  • 1 kudos

Resolved! little fs for stm32h743ii

Dear all,I have dev a custom board  pcb based on stm32h743ii with 32MB of flash and 32MB  sdram FMC  for a 7 inch lcd HD. I am new on cubeide i coming from esp32 world and i have some programing dev question .Is it a good idear to implement :To parti...

KNaim.1 by Associate III
  • 1787 Views
  • 3 replies
  • 0 kudos

Exit from STOP2 mode in STM32u5g7

I am working with the STM32U5G7 microcontroller and have successfully implemented entry into STOP2 low-power mode. My system clock is 80Mhz(HSI, PLL), However, upon wake-up triggered via LPTIM . LPTIM is configured as counts internal clock events wit...

_Danny_ by Associate III
  • 1517 Views
  • 3 replies
  • 2 kudos

STM32H745 parallel transmission

Hi, I have Interface (type MASTER) 10-bit + CLK, FCLK=~9MHzCan I use DCMI to read 10-bit without VSYNC and HSYNC?Or some other method? The usual assembler software method "ldr r1, [port, #....]" is too slow and despite many attempts it has not been p...

EsKi by Associate II
  • 1888 Views
  • 5 replies
  • 0 kudos