STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

read 8 channels from ADC2 in regular mode

Hi,While I can read one channel from both ADC1 & ADC3 in injected interrupt mode, till can not find a solution to read 8 channels from ADC2 in regular mode. Please send me sample code.Thanks

ARost.2 by Associate II
  • 2571 Views
  • 5 replies
  • 0 kudos

Problem setting registers on I2C slave device

I've read through a couple other posts but haven't fount anything that helps me. I am trying to set some registers on a MMC5883 digital magnetometer and can't seem to write to the correct registers. I initialized I2C1 using the graphical Device Confi...

CGrov.1 by Associate II
  • 2105 Views
  • 8 replies
  • 0 kudos

STM32H747I-DISCO programming

Hello, I just got STM32H747I-DISCO board. I have stlink-2 and I guess I cannot program this board with stlink2. Do I need to get STLink-3 or STLink-4 in order to program this board? In the description it says: Board has a built in STLink-v3 inside of...

GunkutA by Senior
  • 4768 Views
  • 13 replies
  • 0 kudos

Resolved! STM32F7 Thermal Reset

We have had trouble with a STM32F7769BGT6 resetting when heated to around 45°C. The part should be rated for 85°C, as are the rest of the components on our board. We've looked at the power supplies and they don't show any issues. To duplicate the pro...

SPI Communication with LTC6803-2

Hello, I'm trying to make a battery management system with LTC6803 but i can't read any values at all. All libraries i found are based on Arduino and i don't have any Arduino which i can try if are they working (so i can try porting the code to STM)....

PPatl.1 by Associate
  • 1171 Views
  • 0 replies
  • 0 kudos

STM32G0 READ AND WRITE ISSUE

Hello,I am using STM32G070CBT6 Controller. I am trying to write and read in 63rd page of flash memory . HAL_FLASH_Unlock(); __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP  |             FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR); FLASH_PageErase(63); HAL_St...