STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Print to Serial port of an STM32F030F4P6

Hi.I have a diy board with STM32F030F4P6 Atollic TrueSTUDIO 9.3.0 and STM32CubeMX 5.2.1.I want to use it 's serial port in order to print (for debugging), like in Arduino we use the Serial.print().I 've followed a few things I found on the internet b...

openOCD by STM

Hello,Is there a version of openOCD compiled by STM which contains all the latest cards (notably the NUCLEO-G071RB) and is it possible to obtain the command generated by STM32CubeIDE configured with openOCD.Because I would like to use another IDE (CL...

ADEVL.1 by Associate II
  • 12216 Views
  • 17 replies
  • 0 kudos

Resolved! Openocd not working with STM32F750

I was successfully using openocd with GDB with STM32F746-DISCO. However, my new STM32F750-DISCO does not work.I use this commands:openocd -f /usr/share/openocd/scripts/board/stm32f7discovery.cfg telnet localhost 4444 reset halt flash write_image eras...

KMaen by Associate III
  • 1425 Views
  • 1 replies
  • 0 kudos

Can the ADC operation frequency be more than 60Mhz?

According to the spec, it says the ADC clock frequency is up to 60Mhz for a single channel. Does it mean we cannot apply the ADC clock more than 60Mhz to the ADC modules? But in the STM32Cube example code, the ADC clock applied to the ADC module is ...

0690X00000Bw7NHQAZ.jpg
LHsu.1 by Associate
  • 2874 Views
  • 4 replies
  • 0 kudos

I'm in the first steps of my project. Selected STM32F446ZE Nucleo board for developing MIC ARRAY application as 446ZE used in BLUECOIN and made my own same arranged mic array board. Now I found there is no Beam Forming sample for it! What to do now?

There is a document about MIC ARRAY BEAM FORMING by ST that suggests DFSDM in found other chip. I'm confused, why bluecoin used same mic array arrangemt but other mcu? How can I find samples for it?

_behn4m by Associate II
  • 813 Views
  • 0 replies
  • 0 kudos

What's wrong with my SPI setup?!

Hi,I'm really struggling with the simplest possible way to use SPI with STM32F745 as a master and a MPU6000 as a slave - no interrupts, no DMA, just plain while loops and busy waiting.Problem: I can't get it to work, the SCK signal is plain dead!Code...

CGalv by Associate III
  • 3698 Views
  • 7 replies
  • 0 kudos

My virtual comport is not recognized by Device Manager.

I need some help. I have a design that uses the STM32F407zgt. Up to now every thing has been going prefectly.  I started my design using the STM32F407VGT or the Discovery board as my breadboard / proof of concept. With the 407VGT, I was able to crea...

MBang.1 by Associate II
  • 3122 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.