STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G4 ADC running in low speed

The new STM32G474RE has an ADC that can run up to 4MSPS.I'm doing a project where I need to do the sampling in 1MSPS. But the maximum sample rate achieved was 300kSPS. When I set timer 1 for the ADC trigger to 500kSPS the "while" loop simply locks. S...

AStaa.1 by Associate II
  • 2308 Views
  • 7 replies
  • 0 kudos

STM32L073z-eval 32.768 LSE issue

Hello, i have some trouble with my L073z-eval board. I try to use RTC with LSE and found it very inaccurate. I checked the frequency using TIM21 (capture-compare mode with remapped LSE as input) and see very instabbility value - some times value goes...

AChas.1 by Associate II
  • 1782 Views
  • 3 replies
  • 0 kudos

Resolved! Can the PC2_C pin be used for digital I/O (STM32H743)

This seems very confusing. In the manual the pin is marked ANA which it annotates as Analog-only input, and yet it has a bunch of special functions that are digital in nature (e.g. SPI_MISO, FMC_SDNE0) and both input and output. CubeMX allows me to s...

PMath.4 by Senior III
  • 4015 Views
  • 6 replies
  • 0 kudos

Resolved! STM32F3 - what is ITR2 for TIM3?

RM0316 says it's TIM5:but there's no TIM5 in the 'F3 (except 'F373, to which RM0316 does not apply).ST please clarify.JWPS. Textual search finds TIM5 also in description of the TIMx_CCRx registers, obviously copy-paste relics.

0690X00000BwHD2QAN.png