cancel
Showing results for 
Search instead for 
Did you mean: 

Not able to do Chip erase on STM32H750VBT6 Internal flash

VAgga
Associate II

Hi,

I am new to STM32 H7. I designed 1 board using STM32H750VBT6. But when i try to erase internal flash using keil IDE, it is showing 'Flash Timeout: Reset the target and try it again'. I have attached the scrennshot of the error.

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

I'd probably try the STM32H7x_2M flash algorithms.

Consider the type of pod you're using, and if it has most current firmware running on it.

Does the board work with the STM32 Cube Programmer?

>>I am new to STM32 H7. I designed 1 board using STM32H750VBT6

Have you tried a NUCLEO or DISCO board with the H7, or went straight to a PCB?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Check supplies, capacitors/voltages on VCAP.

Not familiar with your custom design.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

i am using U-Link2 debugger for erasing the code. Does STM32 Cube programmer supports ULINK.

Here is my design file.

It does not. You'd perhaps want to look at the ST-LINK/V3 pods

Check voltages presenting on VCAP pins. Supplies in general can impact Flash behaviour.

Had any code running on the board?

If flash is not functioning, one could perhaps run test code from internal RAM

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

We have used 12MHz crystal. Can this be a problem??

I tried using STM32H7x_2M flash algorithms and it is erasing the chip successfully.

Why is it not working with STM32H7x_128K flash algorithms.

I don't know, you'd need to review the source code to understand what it is doing and the expectations it has.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you for your support.