STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Activating USART

Hi, I have a Problem with the NUCLEO-L476RG.I tried to activate USART2.Sending a single Char to a Terminal Programm like Putty or HTERM. I took the guide from the reference Manual on Page 1341. But it wont work.#include "stm32l4xx.h" #include "stm32l...

DKalm.1 by Associate II
  • 1067 Views
  • 2 replies
  • 0 kudos

Configure GPIO on NUCLEO-L476RG without Cube MX

Hello,i want to turn the Green USER LED on. #include "stm32l4xx.h" #include "stm32l4xx_nucleo.h" int main(void) { RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN; GPIOA->MODER |= GPIO_MODER_MODER5_0; GPIOA->ODR |= GPIO_ODR_OD5; }So i activated the cl...

DKalm.1 by Associate II
  • 1992 Views
  • 4 replies
  • 2 kudos

Pin values when RESET is pressed.

Hi all, I'm working with a STM32F303CCT6, and I'm testing the different pin values when Reset is pressed. The Reference Manual says the reset value for GPIO_MODER is 0, so all GPIO are inputs.But I'm testing my MCU (first I erased all memory) and ha...

JAlca by Senior
  • 2787 Views
  • 3 replies
  • 0 kudos

Resolved! Moving code to a different memory sector

I am currently saving user data to sector 7 on a STM32F446 board. I need to move that into one of the 16k sectors to keep the erase times small (would prefer to use sector 0, but any 16k sector will work). I am using a linker script to set up memory ...

ALane.1 by Associate
  • 2206 Views
  • 1 replies
  • 0 kudos

Resolved! How to download a profile in ST33 embedded sim?

please any one explain me how different MNO profile downloaded to eSIM ST33. Which communication is used to communicate with ST33 in order to download a profile ? and how to activate this profile?also i would like to know how remote profile managemen...

DPADI.8 by Associate II
  • 1866 Views
  • 2 replies
  • 0 kudos

I am trying to control esc using STM32F446RE Nucleo 64 board but after uploading the program nothing shows up.I am using timer 2 channel one.

#include "main.h"TIM_HandleTypeDef htim2;void SystemClock_Config(void);static void MX_GPIO_Init(void);static void MX_TIM2_Init(void);int main(void){ HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); MX_TIM2_Init(); /* USER CODE BEGIN 2 */   HAL_TIM_P...

PIngo.1 by Associate
  • 1206 Views
  • 1 replies
  • 0 kudos