cancel
Showing results for 
Search instead for 
Did you mean: 

I was able to enter Low Power without going through low power run? How?

TAkha
Associate

I have the system clock set as 120Mhz. I used the HAL driver code, HAL_PWR_EnterSLEEPMode, to enter Low power sleep mode. However, when it checks if it's in run mode, it doesn't recognise its actually in run mode.

  /* If in run mode, first move to low-power run mode.

    The system clock frequency must be below 2 MHz at this point. */

  if (HAL_IS_BIT_SET(PWR->SR2, PWR_SR2_REGLPF) == RESET)

  {

    HAL_PWREx_EnableLowPowerRunMode(); // this never execute.

  }

When it wakes up, the clock speed is still in 120Mhz?

Can anyone help explain me this behaviour? I am using STM32L4R5QII6P processor.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0