STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Weird problem with UART

I work with STM32L475.First I configure UARTint main(void) { /* Configure the system clock to 80 MHz */ SystemClock_Config(); GPIO_Setup();   USART_Setup(UART4, 115200);   USART_SendInt(UART4, 1234, 1); USART_SendInt(UART4, 0,...

STM32H743: what is the source of adc_hclk?

The reference manual explains how I can select between adc_hclk and adc_ker_ck_input as the clock for the ADC but I can't find what the source is for adc_hclk. It is one of the AHB or APB peripheral clocks but which one? Nowhere in the manual can I f...

PMath.4 by Senior III
  • 972 Views
  • 1 replies
  • 0 kudos

Configure SRAM as non-cacheable in MPU

Hello,In stm32h7 I see in the "System architecture" diagram that SRAM3,SRAM2,SRAM1 are not passing through the cache.Yet, it seems that when using SRAM3 with DMA I must configure it as non-cacheable, otherwise I get junk in data.Can anyone please exp...

ranran by Senior II
  • 2139 Views
  • 3 replies
  • 0 kudos

I am trying to adapt the "USART_Communication_TxRx_DMA USART Transmitter/Receiver example" to my custom hardware using a STM32F439ZIT6 processor.

I'm trying to get this example to work with my custom hardware. The TX works fine. I can't get the RX to work.* This example was developed for the NUCLEO-F411RE board and my processor is an STM32F439ZIT6, not F411. Could this be the problem?* I ha...

svick.1 by Associate II
  • 3620 Views
  • 10 replies
  • 0 kudos

MCU selection

I am looking for an MCU for a new project. Desired features:Ethernet, EEPROM, I2C, UART, SPI, PWM, 1MB flash, USB, ETM, possibly TQFP package, no BGA, operating voltage 3 - 3.6 V, OR 5V, -40C to 85 C operating range. Thanks,Priya

PNada.1 by Associate II
  • 946 Views
  • 2 replies
  • 0 kudos

STM32F7 ADC external TIM1 trigger

Is it possible to externally trigger the ADC in group conversion mode + DMA continually? Nothing I have tried seems to work. It appears that I have to call a software conversion for each synced conversion? ``` LL_ADC_REG_SetTriggerSource(ADC1, LL_A...

_EFrie by Senior
  • 2604 Views
  • 6 replies
  • 0 kudos