cancel
Showing results for 
Search instead for 
Did you mean: 

ST Link External Loader development for STM32F746 board using a QSPI NOR flash from ISSI.

DAmig
Associate II

Hardware tested and functional.Commands modified on QSPI example (STM32Cube_FW-F7_V1.15.0) and the erase, read and write commands are functional.Problem to develop an externa loader, based on STM32F769I-EVAL example(using SW4 and MDK-ARM).The MDK_ARM example has scatter file errors (segment order) and the external loader not recognize the file.I need information how to develop the external loader.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0