User Activity

Hardware tested and functional.Commands modified on QSPI example (STM32Cube_FW-F7_V1.15.0) and the erase, read and write commands are functional.Problem to develop an externa loader, based on STM32F769I-EVAL example(using SW4 and MDK-ARM).The MDK_ARM...
The knowledge base text in widget->Circle shows 4 widgets (Box, Box with Border, Line and Circle) on the SHAPES, and the text indicates: "The Circle is located under Shapes in the TouchGFX Designer."Sorry, but, where is Shapes on the TouchGFX Desig...