cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a method to test/simulate an STM32 SRAM Hardware Parity error on an STM32F302 Microcontroller?

TEric
Associate

With SRAM hardware parity checking enabled is there a way to test/simualte a RAM parity error?

Also according to ARM once the NMI handler function is called then the NMI flag is cleared until the processor reasserts the flag. Will the NMI flag remain set once a hardware parity error is detected?

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0552a/Cihfaaha.html

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

> With SRAM hardware parity checking enabled is there a way to test/simualte a RAM parity error?

I'd say, switch on parity checking, write some data, switch off parity checking, write deliberately parity-different data to the same addresses, then switch on parity checking and read the data from those addresses.

> Will the NMI flag remain set once a hardware parity error is detected?

I'd say, no; IMO the parity checking is performed only at the moment of read from given address.

JW