STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F4-Not seeing an I2C signal

Hi, I'm using an STM32F429 MCU and trying to connect to a sensor through I2C. However, I measured both I2C pins with an oscilloscope and they were not showing any clock pulse or a signal. Here's my code for initiation:void MX_I2C1_Init(void) { hi...

JYang.4 by Associate
  • 1139 Views
  • 1 replies
  • 0 kudos

Let me know SPI communication in Register Level operation

Hi I am trying stm32f429zi discovery board for testing SPI communication​I've successed transmitting and receiving data on ADC chip​But I want know "How do these datas going so well?"​So I checked __HAL_SPI_TRANSMIT function​So I found that hspi->ins...

SKim.1761 by Associate III
  • 656 Views
  • 1 replies
  • 0 kudos

STM32G431 AN2606 discrepancy

The datasheet for the STM32G431 (DS12589 Rev 2) shows that the I2C3 peripheral is available on pins PC8 and PC9, but on page 206 of AN2606 Rev 42 it says that the bootloader is using PC6 and PC7 for I2C3. Since STM32CubeMX 5.5.0 agrees with the data...

galens by Associate II
  • 1092 Views
  • 1 replies
  • 2 kudos

Cannot access memory of peripherals

Hello everyone,I am working with STM32H755ZI,, ARM GCC and J-Link GDB.Considering Reference Manual the H755ZI has following Memory Map (cutout):...0x40007C00 - 0x40007FFF UART8 0x40007800 - 0x40007BFF UART7 0x40007400 - 0x400077FF DAC10x40006C00 -...

MBos.1 by Associate II
  • 5203 Views
  • 11 replies
  • 0 kudos

What to use for HAL_SAI_Receive Size parameter?

Hi, I'm trying to work with the SAI HAL interface, i have set the black frame to 64 bits wide and the block slot size to 32B.When using the HAL_SAI_Receive() function, what does the length parameter represent?For my solution i am sending 2 32bit slot...

RBamf.1 by Associate III
  • 1170 Views
  • 1 replies
  • 0 kudos

STM32F74 vs STM32F7: Dual Bank Mode

I'm trying to get dual bank mode to work on an STM32F74. According to application manual AN4826 all STM32F7 series devices should be able to use dual bank mode. However, the reference manual for STM32F74 doesn't mention dual bank mode or Read-while-W...

NCentI by Associate
  • 738 Views
  • 0 replies
  • 1 kudos

Can you support 216MHz when using STM32F746 1.8V?

Hi all,​I am using STM32F746I want to check if it can be used at 216MHz when using at 1.8V.There is some confusion on the data sheet that makes it difficult to determine. (Attachments)Please help me ~Thank you,Best regards.​Gyosun.

sim20 by Associate II
  • 4168 Views
  • 6 replies
  • 0 kudos